AnsweredAssumed Answered

SRC Pairs on ADAU1442/5

Question asked by MagicRuB on Jan 20, 2011
Latest reply on Jan 31, 2011 by BrettG

Is there a requirement to use the SRC's in order on the ADAU1442 or 1445? When using SRC pair 0 in and out, I get data just fine. When using ASRC pair1 while pair0 is unused the data stops. Pair 1 starts working when I give ASRC pair0 an input, even if it's unused and has no data going into it.

 

Is this normal?

 

When I see the work "pair" I assume stereo, is that right? Does it have some other meaning relating to a pair (x2) of ASRC stereo channels?

Outcomes