AnsweredAssumed Answered

questions related to ADSP-21364

Question asked by DeepV on Dec 29, 2010
Latest reply on Dec 29, 2010 by DeepV

Posting questions that came through private forum support. Posting the questions and the answers in this post.

 

1)I did the parallel port programming for ADSP 21364 ,but i did not initialize PLL in that still i could find my code working as i had set the PPBUR3 =55.5Mbytes/sec ,how did this happen.my PCLK is not 166 as PLL is not initialized.

 

2)Does visual DSP support unsigned short int,& unsigned char & other similar datatypes.

 

3)I wrote a simple program on visual DSP,it was a simple calculation program no peripherals included when i compiled during linking i gotcould not locate DM range 0x1200000 -0x1203ffE (seg_sram) on target ,what can be the reason?

 

4)For parallel port  16-bit mode, the address rangeis 0x0 to 0xFFFF which is a 128K bytes (32K 32-bit words)how it comes to 128 K it should be 65536 bytes.

Outcomes