AnsweredAssumed Answered

VisualDSP++ 5.0 Update 8, Blackfin BF561, no uint64_t defined

Question asked by ScottDrysdale on Dec 26, 2010
Latest reply on Jan 4, 2011 by CraigG

i have been running update 7 at work for a while without trouble.  i installed 5.0 with update 8 at home (using 90 day test drive license) to get some stuff done in off hours.  when i compile at home, i get errors like:

 

----------------Configuration: CoreA - Debug----------------

..\..\Commands\AccumulateCommand.cpp

"C:\Program Files\Analog Devices\VisualDSP 5.0\Blackfin\include\osal/adi_osal.h", line 508: cc0020:  error:

          identifier "uint64_t" is undefined

  ADI_OSAL_STATUS adi_osal_ThreadGetCycleCount(uint64_t *pnCycles);

 

how do i fix this?  i tried putting "#include <stdint.h>" at the top of the relevant .cpp file to see if it would go away, but get the same error.

Outcomes