AnsweredAssumed Answered

ADV7441A : AV codes insersion

Question asked by lfill on Dec 13, 2010
Latest reply on Dec 13, 2010 by DaveD

Hello,

 

When using the decoder ADV7441A programmed to generate AV codes, the RGB range is forced to 1-FE to avoid any confusion with the AV codes 0 and FF. But if the decoder also outputs the DE signal, the confusion could be avoided without that the decoder would restrict the RGB range.  Is there a way to program the decoder to generate the AV codes and keep the full RGB range ?


Thanks very much!

Outcomes