AnsweredAssumed Answered

EKIT01-HMC830LP6GE Manual Override

Question asked by kotoo@fujiele.co.jp on May 11, 2015
Latest reply on May 21, 2015 by kotoo@fujiele.co.jp

EKIT01-HMC830LP6GE is used.

I would like to use Manual Override and I would like to output 160MHz by Integer Mode.

 

==Environment==

Hardware:EKIT01-HMC830LP6GE

Software:PLL Eval Software V3_2_4_0 and V3_2_5_0(The problem has occurred by both.)

OS:Win7 32bit

 

==The first confirmation==

The current value of the power supply is confirmed (current value of the stabilizing supply).

=>[I do not remember an accurate value but 0.2-0.3A]

It confirms it by 00h register reading with this software.

=>[Device ID A7975]

Writing and read backing to 02h register

=>[The read buck value is a written value.]

===========================

 

Please teach me Manual Override setting.

I tried it but it is not good.

Please check attachment file.

 

Thank you.

Attachments

Outcomes