AnsweredAssumed Answered

ADSP 21364 -Miscellaneous interrupt.

Question asked by CD30 on Dec 9, 2010
Latest reply on Dec 9, 2010 by Mitesh

Hi,

 

      1)   I am trying to use  MISCB3_I   interrupt ,i have done the SRU configuration for that but i dont understand how to write interrupt signal for that,as in the programmable interrupts there are P0I & P012I for DAI which one to be used for MISCB3_I or if not this way then how?

 

 

2)When will this kind of interrupt go into the ISR ,like when the signal on that particular pin becomes high or how ?

 

3)I want to interface ADIS163xx with ADSP213xx ,connect the reset pin of ADIS with ADSP,how do i do that do i need to do some sru/dai,one thing the reset pin of ADIS is not connected to any of flags of ADSP.

 

 

thanks

 

Outcomes