AnsweredAssumed Answered

Fmcomms5 on VC707

Question asked by MaxPayne on May 7, 2015
Latest reply on May 10, 2015 by MaxPayne

Hello,

 

I'm trying to extend the fmcomms2 solution on VC707 to run fmcomms5 on VC707.

 

Would it be better to implement two fmcomms2 cards for a 4x4 system instead of a fmcomms5?

 

Also can the Linux drivers notice that there are two AD9361s connected to the device? Can the SPI drivers use the chip select to reache the second AD9361?

(Assuming the device tree and the HDL are properly initiated)

 

Regards,

Max

Outcomes