AnsweredAssumed Answered

ADV8003 PiP resolutions?

Question asked by richardbern on May 6, 2015
Latest reply on May 14, 2015 by richardbern

Hi

We are looking into the ADV8003 for a new project that involves Picture in Picture and OSD.  I looked at the eval board and note that there is only a single HDMI input so not sure how we would test PiP features so thought I'd just ask here...

 

Is the size/resolution of the PiP restricted in any way or can we make this as big or small as we want when PiP is active?  Could it be as big as the input 1 resolution if we needed? 

 

Also, are we able to define which of the audio inputs is passed through while PiP is active?

Thanks

Richard

Outcomes