AnsweredAssumed Answered

External OSD 1080p not blending properly.

Question asked by Saurabh_Namjoshi on May 6, 2015
Latest reply on May 7, 2015 by JeyasudhaMuthuPerumal

Hi,

I have modified ADI reference code (V1.90.2) to support my customized hardware. 

I can see external osd in pipmode 5, I have also set alpha for the external osd & it is also working fine.

Input resolution is 1080p from RX(Adv7625), as well as from external osd (Adv7619).

I have modified customized OSD function as we don't have flash for storing OSD binary.

I am only using exosd page create function for exosd.

When I create exosd page with 720p resolution & osd size set to 1080p,it work fine for me.

But when I create exosd page with 1080p resolution & osd size set to 1080p, issue here is it won't work & video is off poor quality mostly video is shaky.

I need to set size of exosd to 1080p.

 

Is the OSD only supports 720p or else what kind of modifications I need to do in the code to support 1080p exosd video size?

Can you help me on this.

 

 

Thanks & regards,

Saurabh

Outcomes