AnsweredAssumed Answered

ERROR: [IP_Flow 19-3461] Value 'IIC_MAIN' is out of the range for parameter 'IIC Board Interface(IIC_BOARD_INTERFACE)' for BD Cell '/axi_iic_main' . Valid values are - Custom

Question asked by BruceZhao on May 4, 2015
Latest reply on May 5, 2015 by BruceZhao

Currently i'm using zed+ fmcomms2 and Vivado 2014.4

I met an error  following the instruction of Building vivado project

the error message is :

ERROR: [IP_Flow 19-3461] Value 'IIC_MAIN' is out of the range for parameter 'IIC Board Interface(IIC_BOARD_INTERFACE)' for BD Cell '/axi_iic_main' . Valid values are - Custom
INFO: [IP_Flow 19-3438] Customization errors found on '/axi_iic_main'. Restoring to previous valid configuration.
INFO: [Common 17-17] undo 'set_property'
ERROR: [Common 17-39] 'set_property' failed due to earlier errors.

    while executing
"rdi::add_properties -dict {CONFIG.USE_BOARD_FLOW true CONFIG.IIC_BOARD_INTERFACE IIC_MAIN} /axi_iic_main"
    invoked from within
"set_property -dict [list CONFIG.USE_BOARD_FLOW {true} CONFIG.IIC_BOARD_INTERFACE {IIC_MAIN}] $axi_iic_main"
    (file "../../../projects/common/zed/zed_system_bd.tcl" line 64)

    while executing
"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"
    (file "system_bd.tcl" line 2)

    while executing
"source system_bd.tcl"
    (procedure "adi_project_create" line 107)
    invoked from within
"adi_project_create fmcomms2_zed"
    (file "./system_project.tcl" line 7)

Is there any advice to work out the problem?

Thanks.

Outcomes