AnsweredAssumed Answered

Can you provide detailed AD9361/9364 Phase Noise performance?

Question asked by BTG Employee on May 4, 2015
Latest reply on May 4, 2015 by tlili

Can you provide more detail on the phase noise of the AD9361/AD9364 transceivers?  There is one bullet for the AD9361 that says 0.25 deg at 2.5 GHz.  Is that the RMS jitter number and if so what are the integration limits?  Ideally, like to get the phase noise at various offsets of 1 kHz, 10 kHz, 100 kHz, and 1 MHz in dBc/Hz.

Outcomes