AnsweredAssumed Answered

ADF4158/9 fsk setting

Question asked by OHDAEHO on Apr 30, 2015
Latest reply on Apr 30, 2015 by rbrennan

I am using the ADF4158 on board with the supplied software.

I would like to create a waveform attached.

Please tell me the settings.

 

In addition, the period of txdata?

 

see also

One. Frequency of 1.3125GHz

Two. Reference Frequency 40MHz

Three. PFD Frequency 20MHz

Four. Was set to R Counter 2.

Attachments

Outcomes