AnsweredAssumed Answered

FMC AD9144 with ADS7-V1

Question asked by SirJanA on Apr 28, 2015
Latest reply on Jul 6, 2015 by Biao.H

Hi,

 

How do I set the appropriate parameters to output one tone above 1 GHz using the FMC AD9144 with the ADS7-V1.  I was able to get it to 1 GHz.

 

Also, I can't get JESD204 PLL Lock when I use an Interpolation Setting of 1.  Why is that?

 

- Jan

Outcomes