AnsweredAssumed Answered

How many possible instructions ADAU1445/1446

Question asked by Robin on Dec 2, 2010
Latest reply on Feb 28, 2011 by JeradL
Branched to a new discussion

I am a little bit confused - the datasheet of the ADAU1445/46 clearly states that the core allows 3584 instructions @ 48 kHz.

However when I read the "compiler_output.txt" file it mentions 4096 possible instructions. Is the difference of 512 instructions reserved for something else? What happens if I load a project that requires slightly more than 3584 instructions  into the DSP?

If I compile such a project I do not get an error message as long as I do not exceed 4096 instructions.

 

Thanks in advance for a quick answer

Robin

Outcomes