AnsweredAssumed Answered

IIO SCOPE CONNECTION TO VC707 WITH FMCOMMS3

Question asked by jsanch on Apr 24, 2015
Latest reply on Sep 8, 2015 by CsomI

Hi,

 

I am having trouble connecting the ADI IIO Oscilloscope to my platform and device.  I am following this guide: http://wiki.analog.com/resources/eval/user-guides/ad-fmcomms2-ebz/quickstart/microblaze.  Here is the hardware I am using. 

 

Xilinx VC707 Kit

AD-FMCOMMS3-EBZ

Micro USB Cable for JTAG connection

Micro USB Cable for UART connection

Ethernet cable

 

1) I have the VC707 Kit connected to a laptop running Windows 7 Pro SP1 (64-bit).

2) I am using Vivado 2014.4.

3) I downloaded vc707_fmcomms2-3_2014_R2_PRE.zip today (Apr 24 2015) and unzipped.

4) I opened the Vivado 2014.4 TcL Shell and typed:

Vivado% xmd -tcl run.tcl

5) It loaded the bit file and the image.  The last few lines in the TcL Shell say:

Setting PC with Program Start Address 0x80000000

Processor started. Type “stop” to stop processor

RUNNING> Disconnected from Target 0

6) I can see the messages from the UART using PuTTY. The last lines are:

Welcome to Buildroot

Buildroot login:

7) I downloaded IIO Oscilloscope (OSC) for Win32 & Win64 (2014_R2 Alpha Pre-Release) adi-osc-setup.exe today (Apr 24 2015) and installed it on the laptop.

8) I launched the Oscope Application and went to Settings → Connect.  The Local Device option is grayed out.

9) I connected an Ethernet cable from the VC707 to the laptop.

10) I typed in the address 192.168.2.2 (shown on the LCD screen of the VC707) in the IP addr:port box.

11) I clicked Refresh and under IIO Devices it says “No iio devices found”.

 

Am I missing a step?

 

Thank you for your help,

 

  Jesus

Outcomes