AnsweredAssumed Answered

Problem with Vref of AD7623

Question asked by Jacky_zhou on Apr 21, 2015
Latest reply on May 6, 2015 by Jacky_zhou

Hi,

      We utilize the internal reference voltage when applying the AD7623. According the datasheet of AD7623, the internal reference voltage is 2.048V, which is produced by the 1.2 V voltage of REFBUFIN pin.


     However, during the test, we test the voltage of REFBUFIN pin is 1.1489V and the voltage of REF pin is 1.864 V, which have a big difference with characteristic of datasheet. Addition, the datasheet only has a typical value of internal reference voltage.

 

    So, is the situation of the introduced above reasonable?

 

Thanks.

Outcomes