AnsweredAssumed Answered

Newbie question on BF532 and external 8-bit memory support

Question asked by Ag56 on Dec 2, 2010
Latest reply on Jan 11, 2011 by CKPATEL

Hi,

 

I have a pretty basic question - forgive me if this is plainly obvious, as I am feeling my way around this still!

 

I am wondering if the BF532 has support for 8-bit external memory on the ASM banks. It seems that it doesn't given the interface is 16-bit, but I wanted to make sure that there's no simple way to make the interface work with 8-bit ROM.

 

So if that is the case, does anyone have a suggestion for a 3.3V operating 4-megabit or so 256x16 flash memory IC to use with the BF532? Performance is not really a premium, just something that will run and is easy to set up. Thanks! Much appreciated.

Outcomes