AnsweredAssumed Answered

AD8128 with a Clamp Voltage

Question asked by Clark197 on Dec 2, 2010
Latest reply on Dec 14, 2010 by Clark197
Hello,
i want to use the AD8128 as an analog Video (ED/HD) receiver and amplifier. I read the Datasheet and see that it have
a DC-Offset Voltage input.
If my video signal already has a DC-Offset, what will happen if i connect a new offset on this pin?
I do not want to have two Offset on the output video.
I want to connect a Clamp Voltage at this pin(I thing it is possible with the AD8129/AD8130).
Thank you

Outcomes