AnsweredAssumed Answered

ADuC7061 ADC1 channel switching

Question asked by P.H.B.A on Apr 20, 2015
Latest reply on Apr 20, 2015 by P.H.B.A

Hi,

ADuC7061 primary ADC can be configured as 2 diff input channels or 4 single-ended input channels, and the aux. ADC can be configured as 4 diff input channels or 7 single-ended. Is there a sample programs code which shows the right way for switching channel on the ADC1 for example, or all I have to do is just wait for the ADC interupt source -> read data form ADC1DAT register -> rewrite the ADC1CON register -> return from interrupt and repeat waiting for the ADC interupt source ? It seems to me that the installation CD does not have it, Thanks for your help in advance.

Best regards.

Outcomes