AnsweredAssumed Answered

AD9144 FMC and FMC DAQ2 for ADS7-V1 or other Xilinx FPGA

Question asked by SirJanA on Apr 15, 2015
Latest reply on Apr 17, 2015 by SirJanA

1)  Can the HDL designs be used in conjunction with the DAC Software Suite?

2)  Can the DAQ2 be used with the DAC Software Suite?

3)  Do you guys have any sample code in using the DAQ2 HDL reference design, non-OS, such as outputting a simple sine wave or receiving one by using UART?

4)  Can the ADS7-V1 be used to synchronize two AD9144 FMC cards?

5)  Can the ADS7-V1 be used to test the FMCDAQ2?

6)  Can two DAQ2 boards be synchronized using the reference designs?

Outcomes