AnsweredAssumed Answered

Dynamic Accuracy ADIS16480

Question asked by Pasha on Apr 15, 2015
Latest reply on Jun 24, 2015 by NevadaMark

Hello, I use the ADIS16480 sensor in the project to determine the pitch and roll angles while driving. I want to know the instantaneous value of the angle to within 1 degree. Currently I'm using Euler Angles. Sensor settings are used by default. By moving the sensor on a flat surface of the table I can see the angles of 5 degrees, and when you move the sensor in a circle within 3-4 seconds values can be Around 15 degrees.
Applications DECIMATION FILTER did not help (use the value DEC_RATE = 245 or 2047).
Which setting is required to obtain a more accurate pitch and roll angles at the required accuracy to 1 degree, the sampling rate of 10 Hz, and the sensor under a moving car?

Outcomes