AnsweredAssumed Answered

Limitation of input current of AD8400 terminals.

Question asked by ysuzuki on Apr 12, 2015
Latest reply on Apr 13, 2015 by DRice

Hello,

 

I have a question about limitation of input current on A, B, W termials of AD8400.

 

In table-5 of the datashee, Absolute Maximum Rating, the current limitation is described as followings. The limitation was changed when the datasheet revision was changed from Rev.D to Rev.E .

 

[Rev.D]

Parameter : IAB Continuous (RAB = 1kohm/10kohm/50kohm/100kohm)

Ratiing   : 5mA / 500microA / 100microA / 50microA

 

[Rev.E]

Parameter : IAB Continuous (RAB = 1kohm/10kohm/50kohm/100kohm)

Rating    : 2.1mA / 2.1mA / 540microA / 540microA

 

I think the Rev.D's description is understandable rather than Rev.E when I consider the maximum input voltage is 5V.

 

Could you teach me why this current limitation was changed from Rev.D to Rev.E ?

 

 

Best regards,

ysuzuki

Outcomes