AnsweredAssumed Answered

IOUT from AD9850

Question asked by raphi on Apr 8, 2015
Latest reply on Sep 30, 2015 by kalupen

Hi,
I'm reading the datasheet of AD9850 and I didn't find the caracteristics of Output signal (pin IOUT). I'd like to know if that signal is symetric or asymetric and in which range it belongs to when Vsupply is 5V and Rset is 3.9K or 1.95K. Does the signal is a 10.24mA.cos(2piFt) or 20.48mA.cos(2piFt) or it is an asymetric signal with that amplitude Peak to Peak ?
Thanks for your answer

Outcomes