AnsweredAssumed Answered

AD9277+CVT-ADC-FMC-INTPZ+Zedboard

Question asked by Mcdull on Mar 31, 2015
Latest reply on Mar 31, 2015 by rejeesh

Hello All,

Please help me with this, really appreciate.

 

I just get AD9277EBZ andCVT-ADC-FMC-INTPZ today, and I have Zedboard in hand. I saw there is a reference design for AD9279 with ML605(http://wiki.analog.com/resources/fpga/xilinx/interposer/ad9279?rev=1353403998), so I am thinking using this as reference and make a design for ad9277 work with Zedboard. I am sure this topic has been discuss several times here, sorry to . I checked FMC header for ML605 and Zedboard, the difference I think is Zedboard do not have pins shown below which I think the clock maps to LA00_CC and the frame + data all within LA01-LA16, is that correct?

P3.C9SD1+C6FMC_LPC_DP0_M2C_PG3MGTRXP0_116116
P3.C10MGTCLK1+D4FMC_LPC_GBTCLK0_M2C_PM6MGTREFCLK1P_115115
P3.D9SD1-C7FMC_LPC_DP0_M2C_NG4MGTRXN0_116116
P3.D10MGTCLK1-D5FMC_LPC_GBTCLK0_M2C_NM5MGTREFCLK1N_115

 

In reference design, there is only bit file and SDK file provided, anyone get a idea of block digram design for Vivado? or is there possible I can get the design file?

 

Thanks a lot

Outcomes