AnsweredAssumed Answered

ADISimRF model for AD6518

Question asked by pbolton on Mar 30, 2015
Latest reply on Mar 31, 2015 by jdobler


Hi All,

 

I am trying to use ADISimRF to gain some insight into the performance of each of the stages in the ADRF 6518 VGA and programmable baseband filter so that I can load it into Spectrasys and model my complete RF strip.

 

The information presented in ADISimRF when you follow the instructions and load in the ADRF 6518 as 8 separate stages for the input IP3 and input P1dB figures don't make sense to me.

 

Currently the model specifies the analog VGA/  VVA component as having an input P1dB at 51 dBm and the input IP3 at 50 dBm when the gain is set to zero. The first stage digital DGA / DSA has an input P1dB at 42 dBm and the input IP3 at 15 dBm when the gain is set to 9.

 

As a sanity check I compared these results with discrete components with similar performance from ADI; the AD8368  (analog VVA plus power detector) and the AD8375 (digital VGA).

 

The AD8368 has a output P1 dB of +16 dBm and an output IP3 of 33 dBm with the gain set to +22 dB. This gives an input P1dB of -6 and an input IP3 of 11 dBm

 

The AD 8375 has an output P1 dB of 19 dBm and an output IP3 of 50 dBm. with the gain set to 20 dB. This gives an input P1dB of -1 dBm and an input IP3 of +30 dBm.

 

Am I loading in the information about the ADRF6518 into ADISimRF incorrectly, or does it have some issues?

 

Regards

 

Patrick

Outcomes