AnsweredAssumed Answered

4K HDMI Receiver and transmitter

Question asked by FreddyS on Mar 29, 2015
Latest reply on Jul 21, 2015 by mattp

Dear Supporter

1. According to the ADV7619 , when the HDMI input is 4K , the TTL output may be at YCrCb 4:2:2 format, 12 bits as following:

 

When setting OP_FORMAT_SEL[7:0] = 0x96

Can you give a clear answer if the HDMI Tx ADV8005 can be connected at the exact same format/way as the ADV7619 RX output and generate 4K on single HDMI port ?

If the TX ADV8005 is not suitable, is there an other 4K HDMI Rx product available?    

 

 

  2. Is there an evaluation board which connects the ADV7619 with ADV8005 using 4K bit map?

 

 

Thanks

Freddy

 

 

Outcomes