AnsweredAssumed Answered

ADV7511 configuration

Question asked by meir.mardechayev@phnx.co.il on Mar 29, 2015
Latest reply on Apr 14, 2015 by Yuvalb

Hello,

 

We would like to activate the ADV7511 in the following mode:

We are using the attache script , but we can not see video.

 

8+8=2xclock per pixel .Adress 0x15 with the value: 01000000

Progressive video,

24 FPS.640X480. – 03C - 01000000

The parallel port is configured to pixel clock of 15.625MHz,  

8+8 bits per pixel (YCrCb), embedded syncs (No FV & LV)

HBlanking is toggling between 13 and 14

VBlanking – 10 before and 10 after.

 

Appreciate if you could check the attached script and help with solution.

 

Thanks

Meir

Outcomes