AnsweredAssumed Answered

ADE7816: Peak detection

Question asked by Mr.K on Mar 26, 2015
Latest reply on Mar 31, 2015 by dlath

Hello,

 

I have a question about the peak detection of ADE7816.

I want to detect the peak of three current channels of A, B, and C.

 

My register setting is shown below.

 

COMPMODE register bit14(CHANNEL_SEL) = 0

 

MMODE register bit2(PEAKSEL0) = 1

               bit3(PEAKSEL1) = 1

               bit4(PEAKSEL2) = 1

 

PEAKCYC register = 0xFF

 

I'm reading the IPEAK register at 5ms intervals.

I think that bit24-bit26 of the IPEAK register is changed one by one.

And I think that only the one bit of bit24-26 is set to 1.

 

Is this correct?

 

I'm setting the PEAKCYC register to 0xFF.

Is the peak detection measured the cycle of 0xFF repeatedly?

 

Best Regards,

Mr.K

Outcomes