AnsweredAssumed Answered

ADR421. Regulator voltage output  is the out of specification under some conditions

Question asked by Dimion on Mar 26, 2015
Latest reply on Apr 15, 2015 by Dimion

Regulator voltage output  is the out of specification under some conditions. Is it posible  what regulator can sets the output voltage to 5,5V if input voltage is 12V and about 4,2 if input is 8V while temperature of enviroment is 85C?

Also, the TRIM input - can it be connected to GND?

Outcomes