AnsweredAssumed Answered

The low input and ouput frequency of the AD-FMCDAQ2-EBZ

Question asked by lan1cao2 on Mar 26, 2015
Latest reply on Mar 27, 2015 by lan1cao2

On the AD-FMCDAQ2-EBZ board the input configuration of AD9680 is differential transformer-coupled.

捕获.JPG

      The frequency range of  ETC1-13-1 is 4.5~3000MHZ . If the input frequency is less than 4.5MHZ, what will happen? Would the input singal suffer a large loss?

    The same question about the AD9144.

        ADT2-1T+: 0.4~450MHZ

        ADTL1-12+: 20~1200MHZ

  If I want to ouput a DC singnal ,would it suffer a great loss?

The signal frequency of my application is from DC,so I

Outcomes