AnsweredAssumed Answered

ADV7611 Driver strength

Question asked by perjos on Mar 25, 2015
Latest reply on Mar 25, 2015 by GuenterL

Hi,

 

In the user guide for ADV7611 it is stated for the settings of the driver strength on the LLC clock that one should choose a value depending on the clock frequency.

 

DR_STR_CLK[1:0]

00     Reserved

01     Medium low (2×) for LLC up to 60 MHz

10     Medium high (3×) for LLC from 44 MHz to 105 MHz

11     High (4×) for LLC greater than 100 MHz

 

What are these recommendations based upon? It must be dependent on the load of the system?

 

Regards,

Per

Outcomes