AnsweredAssumed Answered

Unable to handle kernel paging request

Question asked by Daniel_Camara on Mar 25, 2015
Latest reply on Apr 17, 2015 by Daniel_Camara

Hi people,

  I am trying to test the FMCOMMS4 with a zedboard, but I am unable to run the simplest test.

 

I download newest image (6 February 2015 release (2014_R2)):

http://wiki.analog.com/resources/tools-software/linux-software/zynq_images

 

For the configuration FMCOMMS4 + zedboard I used the boot files that are stored in zynq-zed-adv7511-ad9364-fmcomms4.

 

The image and everything else are the standard from the image, I didn't change anything.

the gunzip -c /proc/config.gz | grep ADV7  returns:

CONFIG_VIDEO_ADV7604=y

CONFIG_DRM_ENCODER_ADV7511=y

CONFIG_SND_SOC_ADV7511_HDMI=y

 

However when I boot I get the following error :

 

*******************************

Unable to handle kernel paging request at virtual address 6c707478

pgd = cd4d4000

[6c707478] *pgd=00000000

Internal error: Oops: 5 [#1] PREEMPT SMP ARM

Modules linked in:

CPU: 0 PID: 2126 Comm: FMComms2/3/4 Not tainted 3.17.0-gd302e45 #1

task: df566940 ti: cd6d6000 task.ti: cd6d6000

PC is at strnlen+0x1c/0x30

LR is at string.isra.7+0x2c/0xc0

pc : [<c0189744>]    lr : [<c018ad44>]    psr: 200f0013

sp : cd6d7e28  ip : 00000000  fp : cd6d7e9c

r10: ffffffff  r9 : c041dabc  r8 : 00000000

r7 : 6c707478  r6 : ffffffff  r5 : ffffffff  r4 : df61f000

r3 : 6c707478  r2 : 6c707478  r1 : 6c707477  r0 : 6c707478

Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 18c5387d  Table: 0d4d404a  DAC: 00000015

Process FMComms2/3/4 (pid: 2126, stack limit = 0xcd6d6240)

Stack: (0xcd6d7e28 to 0xcd6d8000)

7e20:                   cd6d7e98 df61f000 df61f000 c053b2c9 209e0fff c018bfd0

7e40: ffffffff ffffffff 00000000 00000000 df790600 c062c4e8 ff0a0004 ffffffff

7e60: df740018 df740010 df61f000 c062c4e8 df740190 df61f000 df740018 cd711880

7e80: cd6ff400 c018c620 df61f000 cd6d7e98 c0329ccc c053b2c7 6c707478 c04580ac            

7ea0: 00100073 b5bb8000 d6921ac0 cd6cdfa8 b5bb9000 00000001 00000000 c00a6040          

7ec0: cd6e1358 00000000 00000000 c062c4e8 c042f230 00001000 00000fff c01fd7e4            

7ee0: c01fd7c8 d6b17e00 c042f230 c0109284 00000000 cd6d7f20 d6b17e00 00000001           

7f00: b1bff0f4 000ff000 cd6d7f80 c0107f9c c0107f78 c00d46bc cd6d6020 d6b17e30            

7f20: 00000000 00000000 cd6ff400 b1bff0f4 000ff000 cd6ff400 b1bff0f4 cd6d7f80

7f40: cd6ff403 000ff000 b1bff0f4 00000000 b2d2ce90 c00b81f4 cd6ff400 b1bff0f4

7f60: 000ff000 00000000 00000000 cd6ff400 cd6ff403 000ff000 b1bff0f4 c00b880c

7f80: 00000000 00000000 000ff000 00000000 000fff14 b2dccea8 00000003 c000dfe4

7fa0: cd6d6000 c000de60 00000000 000fff14 00000009 b1bff0f4 000ff000 00000000

7fc0: 00000000 000fff14 b2dccea8 00000003 000fff14 b1bff0f4 00058ba8 b2d2ce90

7fe0: 00000000 b2cfe238 b6b6292b b6b62932 80010030 00000009 00000000 00000000

[<c0189744>] (strnlen) from [<c018ad44>] (string.isra.7+0x2c/0xc0)

[<c018ad44>] (string.isra.7) from [<c018bfd0>] (vsnprintf+0x1b0/0x340)

[<c018bfd0>] (vsnprintf) from [<c018c620>] (sprintf+0x1c/0x2c)

[<c018c620>] (sprintf) from [<c0329ccc>] (ad9361_phy_show+0x9c/0x324)

[<c0329ccc>] (ad9361_phy_show) from [<c01fd7e4>] (dev_attr_show+0x1c/0x48)

[<c01fd7e4>] (dev_attr_show) from [<c0109284>] (sysfs_kf_seq_show+0x94/0xf4)

[<c0109284>] (sysfs_kf_seq_show) from [<c0107f9c>] (kernfs_seq_show+0x24/0x28)

[<c0107f9c>] (kernfs_seq_show) from [<c00d46bc>] (seq_read+0x1a4/0x3f0)

[<c00d46bc>] (seq_read) from [<c00b81f4>] (vfs_read+0x88/0x138)

[<c00b81f4>] (vfs_read) from [<c00b880c>] (SyS_read+0x3c/0x7c)

[<c00b880c>] (SyS_read) from [<c000de60>] (ret_fast_syscall+0x0/0x30)

Code: e1a02003 1a000001 e0600002 e12fff1e (e5d2c000)

---[ end trace e7181b299783f454 ]---

****************************

 

  Some one knows where I should start to search?

Outcomes