AnsweredAssumed Answered

ZEDBOARD + FMCOMMS2  ISE 14.4 Reference Design

Question asked by marcob on Mar 23, 2015
Latest reply on Mar 23, 2015 by rgetz

Hi,

 

I've some problems with the zedboard-fscomms2 reference design.

I've checked out 2014_R1 branch for linux sources, downloded firmware fpgahdl_xilinx-ad_fmcomms2_ebz_edk_14_4_2013_10_22.zip.

I've compiled .xco IP : ad_dcfilter_ , ad_dds_1.

 

The compilation is succesfull with XPS/ISE 14.4 , but when the system Boot i've the message :

ad9361 spi32766.0: ad9361_dig_tune: Tuning RX FAILED!

ad9361 spi32766.0: ad9361_dig_tune: Tuning TX FAILED!

 

when I use the .bit file without compilation of firmware section , the system boot is correct, and the

system work fine.

 

Are there firmware / software update to work properly ?

 

Thanks

Outcomes