AnsweredAssumed Answered

AD9467-FMC Error Ref design: ERROR: [BD 5-216] VLNV

Question asked by Carlo75 on Mar 22, 2015
Latest reply on Mar 28, 2015 by Carlo75

Hi!

 

I get this error when I try to run ref-design. What do I do worng?

ERROR: [BD 5-216] VLNV <analog.com:user:util_i2c_mixer:1.0> is not supported for this version of the tools.

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

HW ADI: AD9467-FMC

HW Xilinx: ZedBoard

 

Vivaldo version 2014.2 (64-bit)

 

I downloaded the HDL folder 2015-03-22

analogdevicesinc/hdl · GitHub

 

Work flow

cd c:/AD9467/hdl_master/library/axi_ad9467/

source ./axi_ad9467_ip.tcl

 

I get warnings! Is this ok or need to be fixed?

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/AD9467/hdl_master/library/common/up_xfer_status.v' appears to be outside of the project area c:/AD9467/hdl_master/library/axi_ad9467.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/AD9467/hdl_master/library/common/up_xfer_cntrl.v' appears to be outside of the project area c:/AD9467/hdl_master/library/axi_ad9467.

.

.

.

CRITICAL WARNING: [IP_Flow 19-459] IP file 'c:/AD9467/hdl_master/library/common/up_adc_common.v' appears to be outside of the project area c:/AD9467/hdl_master/library/axi_ad9467.

 

cd c:/AD9467/hdl_master/projects/ad9467_fmc/zed/

source ./system_project.tcl

 

ERROR: [BD 5-216] VLNV <analog.com:user:util_i2c_mixer:1.0> is not supported for this version of the tools.

ERROR: [Common 17-39] 'create_bd_cell' failed due to earlier errors.

 

 

    while executing

"create_bd_cell -type ip -vlnv analog.com:user:util_i2c_mixer:1.0 sys_i2c_mixer"

    invoked from within

"set sys_i2c_mixer [create_bd_cell -type ip -vlnv analog.com:user:util_i2c_mixer:1.0 sys_i2c_mixer]"

    (file "../../../projects/common/zed/zed_system_bd.tcl" line 66)

 

 

    while executing

"source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl"

    (file "system_bd.tcl" line 2)

 

 

    while executing

"source system_bd.tcl"

    (procedure "adi_project_create" line 107)

    invoked from within

"adi_project_create $project_name"

    (file "./system_project.tcl" line 7)

Outcomes