AnsweredAssumed Answered

Input voltage of absolute maximum ratings for ADCMP580, ADCMP581 and ADCMP582

Question asked by ahata Employee on Mar 19, 2015
Latest reply on Mar 26, 2015 by ahata

Hi,

 

I have a question about ADCMP580/1/2.

 

When I see the absolute maximum ratings, Input voltage should be between -3V to 4V.

I believe this means ADCMP58x aren't broken when users use within the ratings.

 

My question is that the AMR of input voltage range is not related to supply voltage range.

I look like even if VCC = 3V, VEE = -3V and Input voltage = 3.9V, ADCMP58x work very well (and it will not be caused from the failure).

 

Is my understanding correct? or User have to set input voltage within power supply?

Outcomes