AnsweredAssumed Answered

sawtooth generator

Question asked by Fritz1 on Mar 19, 2015
Latest reply on Mar 23, 2015 by krisf
Is there a device similar in structure to the ADM 6326 which I can use at the output of an OP amp integrator  (capacitor feedback) which will zero the output of the integrator when it reaches a given threshold. The input to the integrator is  a ~ 10 nsec 25%  pulse at a 6 Mhz rate and the resulting sawtooth is in the frequency range 1 Hz to 100 kHz. The switch itself should be a mosfet device, for zero offset voltage.

 

 

 

Outcomes