AnsweredAssumed Answered

PWDN mode of AD9434

Question asked by sin on Mar 18, 2015
Latest reply on Mar 27, 2015 by sin

Hi all
I have some questions about AD9434.
Q1)

Is it possible to connect pin 29(=PWDN) to DRVDD(high) or AGND(low) directly ?


Q2)

In the additional standby mode, which should I connect pin 29 to, high or low ?

Is AD9434 automatically in the additinal standby mode when clock rate falls below 50MHz ?

 

Best Regards,

Outcomes