AnsweredAssumed Answered

AD9361 IP Core Zynq BRAM ReductionAD-FMCOMMS3-EBZ

Question asked by jlavie on Mar 17, 2015
Latest reply on Apr 8, 2015 by rejeesh

I am using two AD9361 devices on a hardware platform based on the Zynq 7Z030. When I instantiate the IP core axi_ad9361 into the design (from the AD-FMCOMMS3-EBZ reference design), the IP core consumes 64 BRAM36s per core. So using two IP cores consumes 128 of the 265 available BRAM36s (48%).

 

Is there a way to configure the AD-FMCOMMS3-EBZ IP or modify the IP to reduce the number of BRAMs needed to implement the IP design?

 

Thanks for your help!

John

Outcomes