AnsweredAssumed Answered

ADN8810-Configuration of RESET and SB in Parallel Config.

Question asked by sebastian.B on Mar 17, 2015
Latest reply on Mar 17, 2015 by Dongfeng

Hello,

i use 8 ADN8810 for additional output current, in a setup were i need up to 4 channels each with max. 600mA.

Each 2 ADN8810 for one Channel were assembelt like the example in the Datacheet:
"USING MULTIPLE ADN8810S FOR ADDITIONAL OUTPUT CURRENT"
But in there i dont get clearly information about pin SB and RESET in this
mode. Normaly they are set Aktive High or Low, cause they are negeted. But which state mades the ADN8810 to Process my Signal.

Reset on the 5V?

 

Regads Sebastian



Outcomes