AnsweredAssumed Answered

AD9361 and Model  loopback query

Question asked by Cman Employee on Mar 13, 2015
Latest reply on Mar 13, 2015 by dpu

Hi

 

On behalf of customer again. Please advise.

 

Regards,

Ching

 

 

 

 

** Model ** loopback

I have tried to build up a loopback in the model. For this I have copied together the TX and the RX model. The signal path is then as follows:

TX signal source >> AD9361_TX AD9361_RX >> RX baseband signal sink

When I try to run this model, I get the following error message:

"Test signal sample time and filter configuration are not consistent"

The Diagnostic Viewer shows me also where the error occurs:

, Untitled / ADI9361_rx / VerifySampleTime / Assertion '

Is this the expected behavior I should get? If so, is it somehow possible to simulate a loopback or is this not possible because of implementation reasons?

 

 

Outcomes