AnsweredAssumed Answered

Parameters of ad9523 in fmcomms1

Question asked by Jetmiri on Mar 11, 2015
Latest reply on Mar 17, 2015 by DragosB

Hi all,

 

The output clocks at channels 12 and 6 of ad9523 in FMCOMMS1 are always the same. These channels are related with the DAC CLK and DAC DCO. So I should have at least double of clock output of channel 6 in channel 12 in order to sample in the right way.

 

Which parameters should I change in order to have different outputs (to double the output frequency at channel 12)!?

 

Regards,

jet

Outcomes