AnsweredAssumed Answered

AD9361 MATLAB Model - AGC Fast Attack Mode

Question asked by obruendl on Mar 11, 2015
Latest reply on Mar 16, 2015 by mhennerich

I am currently designing a Bluetooth system using the AD9361. Since the transmitter is powered down between packets, I need to use the AGC fast attack mode to adjust the Rx gains at the beginning of each packet. Since carrier is transmitted only a very short time before the packet starts, the AGC setup is quite critical, so I would like to simulate it.

 

Obviously only AGC slow attach mode and manual gain control are implemented in the AD9361 MATLAB model. Are there any other resources to simulate the AGC fast attack behavior (specialized MATLAB models, etc.)?

 

Regards,

 

Oliver

Outcomes