AnsweredAssumed Answered

AD9467-FMC-250EBZ integrated logic analyzer no data

Question asked by andrewwang on Mar 10, 2015
Latest reply on Jan 4, 2016 by CsomI

Hi Istvan,

 

I followed the wiki page for the ad9467 for a KC705 and was able to compile the hdl and C code onto the board and see the tests run on the UART. However, when I open the hardware manager and try to see the data from the ILA I get all 0's.

 

What I did was:

 

1) synthesized, implemented, generated bitstream, and programmed the bitstream to the KC705

2) Copied the AD9467 driver, AD9517 driver, and ad9467-FMC-EBZ reference design to an SDK application project

3) ran program and could see on that the ADC board was detected on the UART

4) went to hardware manager in vivado 2014.2 and looked at the ILA but saw that all the values were 0.

 

Did I miss something?

 

Andrew

Outcomes