AnsweredAssumed Answered

HMC6981LS6 power detector circuit

Question asked by sss on Mar 10, 2015
Latest reply on Apr 10, 2015 by sss

Hi,all.

 

Our Customer will evaluate HMC6981LS6.

They have several questions to design the power detector circuits with OP amp.

 

Q1. What is the on-chip power detector diode specification?

, absolute Maximum Rating:forward current and reverse voltage?

, specification for 11pin and 12pin?

 

Q2. In the datasheet 9/10 page application circuits , there is suggested circuit with OP amp.

, how is the specification of recommended OP amp?

, or what is the part number using to evaluate ?

 

Best Regards,

sss

Outcomes