AnsweredAssumed Answered

ADuM6000 EMI @ 180 MHz

Question asked by samsonian on Mar 9, 2015
Latest reply on Mar 12, 2015 by samsonian

My client is currently using the ADuM6000. Apparently after conducting RF Emission testing @ 360MHz their end product is not passing and they believe they have "pinpointed" the emissions coming from the ADuM6000. They also ordered the ADuM6000 eval board and tested it with a 7mA load and RF emission is the same as their board @ 360 MHz. According to them they have followed AN-0971. Any suggestions or tips would be greatly appreciated. Thanks 

 

Sam

Outcomes