AnsweredAssumed Answered

Question of synchronizing multiple AD9910

Question asked by chshwen on Mar 10, 2015
Latest reply on Mar 13, 2015 by sitti

Hi Sir:

 

We reference the CN-0121 for synchronizing multiple AD9910, and met a question need your help.

 

When we got the synchronization signal from AD9910-A, AD9910-B and AD9910-C, then check register of "SYNC_SMP_ERR", AD9910-B and AD9910-C are 0, but AD9910-A is "1", is it correct?

 

By the way, have any suggestions of register setting procedure  for synchronizing multiple AD9910?

111.PNG

 

Thanks and B.R.

Wen

Outcomes