AnsweredAssumed Answered

Absolute max supply voltage rating AD623

Question asked by aerohoff on Mar 9, 2015
Latest reply on Mar 10, 2015 by harryh

Hello,

I'm working with the AD623 and powering it from 12V, which is the top of the power supply operating range (2.7 - 12V). However the absolute maximum supply voltage rating is ±6V (or 12V) so there is no margin between the two.

I'm assuming it's safe to operate the amp at the top of the "operating range". Why wouldn't there be a margin?

The AD8223 is rated the same way. Absolute max is the top of the operating range.

Is there a reason to spec parts this way?

Outcomes