AnsweredAssumed Answered

Can ADV8003 have one HDMI output with OSD one without

Question asked by JonathanMore on Mar 6, 2015
Latest reply on Mar 9, 2015 by mattp

I need the following:

 

- HDMI input. Could be FHD 1080p, 1080i or 720p.

- External OSD input for overlay. Overlay should be able to be anywhere on the screen; assume if overlay value is black, the HDMI comes though 100%. Overlay format could be 800x480 and have to be scaled up, but might be 960 x 540 to make the upscaling easier

 

- HDMI output #1 1080p. Needs to be clone or upscaled version of HDMI input

- HDMI output #2 1080p. HDMI input with OSD overlay

 

Questions:

- Can the ADV8003 do this or do I need the 8005?

- can I do this using the Eval board and some hacking here and there?

 

Thanks. I saw the question about the external OSD how to set the alpha value, glad that was answered.

 

Jonathan More

Outcomes