AnsweredAssumed Answered

Problem with USB connection ADAU1702 Eval Board

Question asked by VicZ Employee on Feb 27, 2015
Latest reply on Feb 27, 2015 by JohnTo

having an issue with the Studio software when downloading the file to EVM board. The message we get is noted below and it may be some setting we are missing as it communicates with board via USB as we can see the registers and mute/unmute andso on.

 

Compiled,Comms Failed

  

The "Compiled: Comms Failed" state occurs when the "Link Compile Download" command is used and compilation is successful but there is an error communicating with the USB device or evaluation hardware.  (This indicator is only available with the second generation EVAL-ADAUSB2 (USBi) interface).

 

 

The schematic status bar color is light orange.

Outcomes