AnsweredAssumed Answered

HMC832

Question asked by ADIguy on Feb 24, 2015
Latest reply on Feb 26, 2015 by dyoung1

Hello,

 

I'm looking to use the HMC832 in the Exact Frequency Mode to generate the frequencies listed below. I would like to know if there is a Greatest Common Denominator (GCD) that can be used to generate these frequencies? Do you have a tool that can be used to determine a GCD and the required PFD? Thanks.

 

Best Regards.

 

774.881118876  MHz

768 MHz.

780.190476192 MHz.

680.4 MHz.

720.0 MHz.

786.432 MHz.

Outcomes